This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CPU timer interrupt priorities in F28335

Hi, 

I am wondering if it is possible to set up different priorities for CPU timer interrupts.

For example, I would like to have cpu0timer > cpu1timer1 > cpu2timer

When CPU timer 0 triggers an interrupt and evoke the interrupt service routine (ISR), it can't be interrupt by timer 1 or time2's interrupts

When CPU time 1  triggers an interrupt and evoke the interrupt service routine (ISR), it can't be interrupt by time2's interrupts but can be interrupt by timer 0

When CPU time 2  triggers an interrupt and evoke the interrupt service routine (ISR), it can be interrupt by timer 0 or timer 1

 

It there any way to do it?

What register should I set up?

 

Thanks a lot!

Alfred