I am trying to stop the PWM from the CLA by forcing a Trip Zone Event, DCAEVT1.
This works perfect from CPU2:
EPWM_forceTripZoneEvent(PWM_Prim1_BASE, EPWM_TZ_FORCE_EVENT_DCAEVT1);
EPWM_forceTripZoneEvent(PWM_Prim2_BASE, EPWM_TZ_FORCE_EVENT_DCAEVT1);
EPWM_forceTripZoneEvent(PWM_Sec1_BASE, EPWM_TZ_FORCE_EVENT_DCAEVT1);
EPWM_forceTripZoneEvent(PWM_Sec2_BASE, EPWM_TZ_FORCE_EVENT_DCAEVT1);
in the board.h file:
#define PWM_Prim1_BASE EPWM1_BASE
#define PWM_Prim2_BASE EPWM2_BASE
#define PWM_Sec2_BASE EPWM4_BASE
#define PWM_Sec1_BASE EPWM5_BASE
when I run the same code from the CLA (in CPU2) nothing seems to happening, the PWM continues to run.
What do I do that´s not correct?
I handle the ADC from the CLA without any problems (ADC_readResult).
Best regards
Kenneth Svensson