This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28067: TMS320F28067 ERROR " _system_post_cinit()"

Part Number: TMS320F28067

/*
 * main.c
 *
 *  Created on: 13-Jul-2023
 *      Author: dsingh
 */

//###########################################################################
//
// FILE:   Example_2806xLEDBlink.c
//
// TITLE:  Timer based blinking LED Example
//
//!  \addtogroup f2806x_example_list
//!  <h1>Timer based blinking LED(timed_led_blink)</h1>
//!
//!  This example configures CPU Timer0 for a 500 msec period, and toggles the
//!  GPIO34 LED once per interrupt. For testing purposes, this example
//!  also increments a counter each time the timer asserts an interrupt.
//!
//!  \b Watch \b Variables \n
//!  - CpuTimer0.InterruptCount
//!
//! \b External \b Connections \n
//!  Monitor the GPIO34 LED blink on (for 500 msec) and off (for 500 msec) on
//!  the 2806x control card.
//
//###########################################################################
// $TI Release:  $
// $Release Date:  $
// $Copyright:
// Copyright (C) 2009-2023 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
//
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the
//   distribution.
//
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
//#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
#include "F2806x_Device.h"     // F2806x Headerfile Include File
#include "F2806x_Examples.h"   // F2806x Examples Include File
//#include "F2806x_Adc.h"
//#pragma CODE_SECTION(epwm1_timer_isr, "ramfuncs");
//#pragma CODE_SECTION(epwm2_timer_isr, "ramfuncs");
////
//// These are defined by the linker (see F2808.cmd)
////
//extern Uint16 RamfuncsLoadStart;
//extern Uint16 RamfuncsLoadEnd;
//extern Uint16 RamfuncsRunStart;
//extern Uint16 RamfuncsLoadSize;
////
// Function Prototypes statements for functions found within this file.
//
//__interrupt void cpu_timer0_isr(void);
//
// Main
//
void main(void)
{
    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the F2806x_SysCtrl.c file.
    //
    InitSysCtrl();
    EALLOW;
//    GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
//      //  GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0;
//    GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;

     //  GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3;

       GpioCtrlRegs.GPBMUX1.bit.GPIO40 = 0;
     //  GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0;
       GpioCtrlRegs.GPBDIR.bit.GPIO40 = 1;
//     //  GpioCtrlRegs.GPBDIR.bit.GPIO41 = 1;
       EDIS;
    //
    // Step 2. Initalize GPIO:
    // This example function is found in the F2806x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    //
     //InitGpio();  // Skipped for this example

    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
    DINT;

    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F2806x_PieCtrl.c file.
    //
    InitPieCtrl();

    //
    // Disable CPU interrupts and clear all CPU interrupt flags
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F2806x_DefaultIsr.c.
    // This function is found in F2806x_PieVect.c.
    //
    InitPieVectTable();

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //
//    EALLOW;    // This is needed to write to EALLOW protected registers
//    PieVectTable.TINT0 = &cpu_timer0_isr;
//    EDIS;      // This is needed to disable write to EALLOW protected registers

    //
    // Step 4. Initialize the Device Peripheral. This function can be
    //         found in F2806x_CpuTimers.c
    //
   // InitCpuTimers();   // For this example, only initialize the Cpu Timers

    //
    // Configure CPU-Timer 0 to interrupt every 500 milliseconds:
    // 80MHz CPU Freq, 50 millisecond Period (in uSeconds)
    //
   // ConfigCpuTimer(&CpuTimer0, 90, 2000000);//4-Seconds

    //
    // To ensure precise timing, use write-only instructions to write to the
    // entire register. Therefore, if any of the configuration bits are changed
    // in ConfigCpuTimer and InitCpuTimers (in F2806x_CpuTimers.h), the
    // below settings must also be updated.
    //

    //
    // Use write-only instruction to set TSS bit = 0
    //
    //CpuTimer0Regs.TCR.all = 0x4001;

    //
    // Step 5. User specific code, enable interrupts:
    //

    //
    // Configure GPIO34 as a GPIO output pin
    //
   // EALLOW;
//    GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
//    GpioCtrlRegs.GPBDIR.bit.GPIO34 = 0;
//    GpioCtrlRegs.GPBPUD.bit.GPIO34=1;

//    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0;
//    GpioCtrlRegs.GPADIR.bit.GPIO18 = 1;


   // EDIS;

//    EALLOW;
//     //  GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3;
//
//       GpioCtrlRegs.GPBMUX1.bit.GPIO40 = 0;
//     //  GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0;
//       GpioCtrlRegs.GPBDIR.bit.GPIO40 = 1;
//     //  GpioCtrlRegs.GPBDIR.bit.GPIO41 = 1;
//       EDIS;


//    //
//     // Copy time critical code and Flash setup code to RAM
//     // This includes the following ISR functions: epwm1_timer_isr(),
//     // epwm2_timer_isr(), epwm3_timer_isr and and InitFlash();
//     // The  RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart
//     // symbols are created by the linker. Refer to the F2808.cmd file.
//     //
//     memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32)&RamfuncsLoadSize);
//
//     //
//     // Call Flash Initialization to setup flash waitstates
//     // This function must reside in RAM
//     //
   //  InitFlash();
//
//    //
    // Enable CPU INT1 which is connected to CPU-Timer 0
    //
    IER |= M_INT1;

    //
    // Enable TINT0 in the PIE: Group 1 interrupt 7
    //
   // PieCtrlRegs.PIEIER1.bit.INTx7 = 1;

    //
    // Enable global Interrupts and higher priority real-time debug events
    //
    EINT;   // Enable Global interrupt INTM
    ERTM;   // Enable Global realtime interrupt DBGM

    //
    // Step 6. IDLE loop. Just sit and loop forever (optional)
    //

    for(;;)
    {
        Uint16 counter=0;
        Uint16 i=0;
//       GpioDataRegs.GPATOGGLE.bit.GPIO18 = 1;//GPIO34
//        DELAY_US(1000000);
        GpioDataRegs.GPBTOGGLE.bit.GPIO40 = 1;//GPIO34
        for(i;i<3000;i++)
        {
            if(counter>=3000)
            {
            break;
            }

            counter++;
        }

      //  DELAY_US(100000);
//        GpioDataRegs.GPBTOGGLE.bit.GPIO41 = 1;//GPIO34
//        DELAY_US(1000000);
    }
}

//
// cpu_timer0_isr -
//
//__interrupt void
//cpu_timer0_isr(void)
//{
//    CpuTimer0.InterruptCount++;
//
//    //
//    // Toggle GPIO34 once per 500 milliseconds
//    //
//    GpioDataRegs.GPATOGGLE.bit.GPIO18 = 1;//GPIO34
//
//    //
//    // Acknowledge this interrupt to receive more interrupts from group 1
//    //
//    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
//}
//
////
//// End of File
////
//
//
//




 

DEAR SIR,

I AM GETTING ERROR WHEN I AM DEBUGING LED BLINK CODE FOR TMS320F28067 DSP CONTROLLER. FOR REFERENCE I HAVE ATTACHED ERROR SCREEN SHOT AND CODE ALSO.KINDLY PROVIDE THE SOLUTION. 

  • Hello Devershi,

    If you look at the Console output when you compile/connect/run the code on your device, do you see any errors or warnings? If you look at the Disassembly view, what is the program currently running? Does this happen with any other examples you try to run on the device?

    Best regards,

    Omer Amir