Part Number: TIDM-02002
Other Parts Discussed in Thread: C2000WARE, PMP21495, PMP21999
The left picture is the schematic diagram of the T100 transformer in the C2000Ware_DigitalPower_SDK_5_00_00_00\ solution \tidm_02002\ hardware, and the right picture is the schematic diagram of the T100 transformer in the reference design of TDM-02002. The two pictures do not agree. The left image is the CLLLC structure and the right image is the CLLC structure. Is one of them wrong? In addition, the T100 turns ratio is not consistent in these two pictures, one is 8:6 and the other is 8:5.