This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: There is a problem with configuration file F320x.json in the TMS28388F1D's sysconfig (17.0.2838).

Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

Hi Team,

There's an issue from the customer need your help:

There seems to be a problem with F1x.json in deviceData in the configuration file in sysconfig (17.0.2838).

The "ID_501" (176pin) and "ID_500" (337bga) positions in the parts node should be swapped, otherwise when using the 337bga model, it will be treated as 176pin, and sysconfig will error when setting IO port #100 or more (except #133, because 176pin has #133), indicating that there is no such port.

Thanks & Regards,

Ben