Part Number: TMS320F28377D
Other Parts Discussed in Thread: UNIFLASH
Hello Support - Team,
I actually have a problem to load the files on to the newest series of boards with the TMS320F28377D.
We built several hundred of this board the last few years without any problem.
Actually we set up a new series of 50pcs and I`m not able to programm one of those.
When i take an old one out of the box it is working as allways known.
During my attempts i recognized that the parts are optically quite differrent.
Maybe you can check it?
one "old" one working
one "new" one not working
Additionally i attach the error message from my uniflash:
[17.10.2023 09:24:31] [ERROR] C28xx_CPU1: Error connecting to the target: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002) [17.10.2023 09:24:44] [ERROR] IcePick_C_0: Power Failure on Target CPU [17.10.2023 09:24:59] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete [17.10.2023 09:25:00] [INFO] C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed. [17.10.2023 09:25:03] [ERROR] C28xx_CPU1: JTAG Communication Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.2.0.00002) [17.10.2023 09:25:04] [ERROR] C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0) [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: File Loader: Memory write failed: Unknown error [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug. [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x5D200@Program: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug. [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [17.10.2023 09:25:24] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected
Kind regards