Part Number: TMS320F280025C
Hello everyone,
I want to read adc voltage in ISR but somehow my isrCount is not increment.
I am using ADCA3/C5
ADC is triggered using epwm1 SOCA...
Note: I run the demo code "adc_ex2_epwm_tempsensor". this code is working fine also isrCount is incremented.
I am attaching a code for your ref. Please check.
//
// Included Files
//
#include "f28x_project.h"
//
// Defines
//
#define RESULTS_BUFFER_SIZE 256
//
// Globals
//
uint16_t sensorSample = 0;
uint16_t isrCount = 0;
int16_t sensorTemp = 0;
//
// Function Prototypes
//
void initADC(void);
void initEPWM(void);
void initADCSOC(void);
__interrupt void AdcA3ISR(void);
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
//
InitSysCtrl();
//
// Initialize GPIO
//
InitGpio();
//
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
InitPieVectTable();
//
// Map ISR functions
//
EALLOW;
PieVectTable.ADCA3_INT = &AdcA3ISR; // Function for Adca interrupt 1
EDIS;
//
// Configure the ADC and power it up
//
initADC();
//
// Configure the ePWM
//
initEPWM();
//
// Setup the ADC for ePWM triggered conversions on channel 1
//
initADCSOC();
EALLOW;
//
// Enable PIE interrupt
//
PieCtrlRegs.PIEIER10.bit.INTx3 = 1;
//
// Sync ePWM
//
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
//
// Enable global Interrupts and higher priority real-time debug events:
//
IER |= M_INT10; // Enable group 10 interrupts
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//InitTempSensor(3.3f);
//
// Start ePWM
//
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOCA
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Unfreeze, and enter up count mode
//
// Wait while ePWM causes ADC conversions, which then cause interrupts,
// which fill the results buffer, eventually setting the bufferFull
// flag
//
while(1)
{
}
}
//
// initADC - Function to configure and power up Adca.
//
void initADC(void)
{
//
// Setup VREF as internal
//
SetVREF(ADC_ADCA, ADC_INTERNAL, ADC_VREF3P3);
EALLOW;
//
// Set AdcaLK divider to /4
//
AdcaRegs.ADCCTL2.bit.PRESCALE = 6;
//
// Set pulse positions to late EOC
//
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//
// Power up the ADC and then delay for 1 ms
//
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
EDIS;
DELAY_US(1000);
}
//
// initEPWM - Function to configure ePWM1 to generate the SOC.
//
void initEPWM(void)
{
EALLOW;
EPwm1Regs.ETSEL.bit.SOCAEN = 0; // Disable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC on up-count
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.bit.CMPA = 0x0800; // Set compare A value to 2048 counts
EPwm1Regs.TBPRD = 0x1000; // Set period to 4096 counts
EPwm1Regs.TBCTL.bit.CTRMODE = 3; // Freeze counter
EDIS;
}
//
// initADCSOC - Function to configure ADCA's SOC0 to be triggered by ePWM1.
//
void initADCSOC(void)
{
//
// Select the channels to convert and the end of conversion flag
//
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0x03; // SOC0 will convert pin A3
AdcaRegs.ADCSOC0CTL.bit.ACQPS = 45; // Sample window is 10 SYSCLK cycles
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; // Trigger on ePWM1 SOCA
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; // End of SOC0 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; // Enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // Make sure INT1 flag is cleared
EDIS;
}
__interrupt void AdcA3ISR(void)
{
isrCount++;
//
// Add the latest result to the buffer
// ADCRESULT0 is the result register of SOC0
sensorSample = AdcaResultRegs.ADCRESULT0;
//
// Clear the interrupt flag
//
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
//
// Check if overflow has occurred
//
if(1 == AdcaRegs.ADCINTOVF.bit.ADCINT1)
{
AdcaRegs.ADCINTOVFCLR.bit.ADCINT1 = 1; //clear INT1 overflow flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
}
//
// Acknowledge the interrupt
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP10;
}