Part Number: TMS320F28379D
Hi,
I am facing difficulties using the loadti to load TMS320F28379D. I am loading the device using the following command:
.\loadti -c NewTargetConfiguration.ccxml HTOL_auto_measurement_1p2.out
It works fine. The problem is that the next time I try the same command it shows the following error:
Configuring Debug Server for specified target...
Done
TARGET: Texas Instruments XDS100v2 USB Debug Probe_0
Connecting to target...
SEVERE: IcePick_C_0: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 9.12.0.00150)
SEVERE: emulation failure occurred
SEVERE: Error connecting to the target: emulation failure occurred
Error code #4
In short, I have to load the program from cmd and load multiple times.
What is the best way of doing this?
Best
Ratul