Part Number: TMS320F28377S
Hi TI expert,
F28377's datasheet shows that VIL(Low-level input voltage)'s min value is Vss-0.3V. I connect Vss to GND. Does it mean that some of the F28377's GPIO commit the input is low level only when corresponding GPIO pin arrive -0.3V?
If I want to trigger external interrupt at falling edge, how much is the minimum voltage for the chip to recognize the falling edge? Is that also -0.3V?

Thanks!
Regards,
Fengyu