Hi
I'm following the FBPS user guide (Phase Shifted Full Bridge) base on EVM: TMDSACDCKIT(C2000 AC/DC Developer's Kit). On page 20 it says:
"23. Power the DC input at J26-J27 with a DC power supply, set to output about 15V or so."
And on page 21 is says:
"25. In each case, after observing the voltages/currents/variables shut down the 15V supply at J26-J27 BEFORE halting the controller.
26. Fully halting the DSC when in real-time mode is a two-step process. With the 15V supply at J26-J27 shut off wait a few seconds. First, halt the processor by using Shift <F5>, or using the Halt button on the vertical toolbar, or by using Debug Halt. Then click Debug Real-time Mode and uncheck the “Real-time mode” to take the DSC out of real-time mode and then reset the DSC."
I'm assuming these instructions are based on some aux-power added on the board. Could anyone tell me where I shall set the aux-power? At J9 (12V aux) or at J10(5V)? I guess maybe I shall implement it at J9(12V). But I'd like to confirm it. Could anyone give me some advice?
Thanks a lot,
Violet