This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-XDS110: Disable VTRef check

Part Number: LP-XDS110
Other Parts Discussed in Thread: LAUNCHXL-F280025C, TMDSEMU110-U

Hello TI,

I want to flash / debug a target without connecting the internal 3.3V supply of the target to the probe. The reason are space constrains...

Using the onboard debugger of a LAUNCHXL-F280025C to debug the target works fine. Anyway, if I use a stand-alone XDS110, it fails with the error 'SC_ERR_XDS110_TARGET_SUPPLY' - of course it cannot sense the internal supply voltage without a physical connection.

Is there a way to disable the VTRef check of the XDS110?

Best regards,

Markus