I cannot flash program our CM firmware into a TMS320F28388S processer using the serial flash programmer and the SCI flash kernel.
I edited all of the flash sections in my linker file to use the ALIGN(8) directive to try to fix the problem but it didn't change the behavior.
Here is the error message I am getting:
Application load successful!
Done waiting for application to download and boot...
SUCCESS of Command
ERROR Status: PROGRAM_ERROR
ERROR Address: 0x204008
Flash API Error: Incorrect Data Buffer Length
Please refer to the Flash API documentation for further explanation of the error.
FMSTAT Register contents: 00
What do I need to do to resolve this issue?