Other Parts Discussed in Thread: C2000WARE
Hello,
I am currently working on a project using the TMS320F28388D, and I'm encountering an issue with initializing a constant array in a specific memory section. My goal is to load a predefined const
array into the CPU1_TO_CM_MSGRAM1
, which is located at the address 0x39400
.
For reference, I am following the example provided in C2000Ware_5_00_00_00\driverlib\f2838x\examples\c28x_cm\flash_kernel
, specifically the file named "flash_kernel_c28x_cm_ex1_sci_boot_cpu1.c"
.
While debugging this using Code Composer Studio (CCS), I noticed that the memory at 0x39400
on CPU1 only contains zeros (0x0000
), instead of the expected array values.
In the first section of my code, I have declared the array as follows:
const uint16_t CopyDataToCMRAM[138] = {
0xB500, ..., 0x400F
};
In the linker command file (.cmd
), I have divided the CPU1TOCMRAM
into two sections:
CPUTOCMRAM_0 : origin = 0x039000, length = 0x000400
CPUTOCMRAM_1 : origin = 0x039400, length = 0x000400
Additionally, the .cmd
file specifies:
MSGRAM_CPU_TO_CM > CPUTOCMRAM_0, type=NOINIT
MSGRAM_CPU_TO_CM_COPY_TO_S0_RAM > CPUTOCMRAM_1, type=NOINIT
I've observed that when I comment out the #pragma DATA_SECTION(CopyDataToCMRAM, "MSGRAM_CPU_TO_CM_COPY_TO_S0_RAM")
, the array is correctly located in the LSRAM and initialized as expected.
My question is: How can I properly initialize an array into the IPC MSGRAM from CPU1 to CM on the 28388D?
Thanks in Advance.
B.D.