Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE
Dear Champs,
I am asking this for our customer.
The user uses internal ref. 1.65V for the buffered DAC, and needs to calibrate offset to the spec like the datasheet for their application requirement.
In TRM,
15.2.2 DAC Offset Adjustment
it says "If the DAC is used at any reference voltage other than 2.5v, the offset trim must be adjusted to ensure the offset error performance stays within the device-specific data manual limits. The DAC offset register is a 16-bit register that contains the 8-bit signed offset trim in the lower half of the register. Use the function call DAC_tuneOffsetTrim() found in C2000Ware to adjust the offset."
Questions:
Would you please show us explicitly how the user set for DACTRIM for negative toward?
For example, they found the offset is 20mV when they set 0 as DAC value, how do they tune?