Part Number: TMS320F28379D
I was trying to see if there is a possibility to use any output from the CLB as an input to the eCAP capture modules (INPUT7 TO 12). I would like to implement a debouncer in hardware using CLB logic and have the CLB output fed into the eCAP inputs. Checking the 28379D datasheet, it seems this is not possible, is that correct? Is there any alternative?