Other Parts Discussed in Thread: C2000WARE
Hi expert,
I need an ICE60730 self-test library for F280049C and F2800137, is there a recommended library?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
I need an ICE60730 self-test library for F280049C and F2800137, is there a recommended library?
There is a diagnostic library in C2000Ware that can help with some IEC 60730 measures. You can look for it in <C2000Ware install location>/libraries/diagnostic.
There's also this app note that can help customers map the standard to the device safety manual diagnostic list.
Whitney
Hi Whitney,
Thanks for your support!
in the:
ti\C2000MCU_IEC60730\C2000MCU_IEC60730_4_00_01_00\IEC60730_STL_Library_v4_00_01_00\IEC60730_STL_Library_v4_00_01_00\IEC60730_safety\v4_00_01_00\source\c28x\STL_spc_detect.c
Where is the _STACK_END (as shown in the diagram) defined and modified?
Is the STL_SPC_DETECT_WPR1_REF_LOW of line 67 misspelled to the point of repeating the definition of line 70? Should it be changed to STL_SPC_DETECT_WPR1_MASK_LOW?


Best Regards
Anka Zhang
Where is the _STACK_END (as shown in the diagram) defined and modified?
The linker generates that symbol based on how the user has configured their .stack section. See the assembly language tools guide.
Is the STL_SPC_DETECT_WPR1_REF_LOW of line 67 misspelled to the point of repeating the definition of line 70? Should it be changed to STL_SPC_DETECT_WPR1_MASK_LOW?
I agree, it does look like it should be MASK_LOW instead of REF_LOW. I'll file a bug.
Whitney