Hello:
A strange problem need help !!
Step by Step :
1.first .my program perform Program is correctly base on the CCS4 Debug Mode (Flash).
2.all Power off and Remove The XDS100V2 from Target Board .
3.Turn on Target Board Power to run 28035 in Stand-alone mode .then 28035 Can Reset and Perform program but not correctly.
it can detect A/D Voltage to starting motor but can't detect A/D Voltage to stop motor .
As this tme. if I pull down XRS PIN to ground Manual after it's Correctly work . (can start & stop motor by A/D Value detect )
4.repeat 3rd step that always occur. why ? Bootloader ? BOR ? ....