This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280038C-Q1: f280038cpmq1

Part Number: TMS320F280038C-Q1

Trouble Reading Register ST1:
(Error -1156 @ 0x6)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
(Emulation package 9.11.0.00128)

how to fixed the issue 

  • Look like device is getting reset. You can check the XRSn pin of device and see if it's toggling. If yes then it may be due to WD reset. Other reason for this error could be that you are putting the device into low power mode via your code. 

    Vivek Singh