This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: gpio

Part Number: TMS320F28035

Hi expert,

Is there a requirement to set the digital and analog pin levels to be low when the chip(F28035 or F2800137) is powered up?

Does the ecap pin of 3.3V affect the power on of the chipF28035 or F2800137)?

In the article *TMS320F2802x/TMS320F2803x to TMS320F28002x Migration Overview, 6 Power Sequencing. It says ‘’Before powering the F28002x devices, no voltage larger than 0.3 V above VDDIO can be applied to any digital pin, and no voltage larger than 0.3 V above VDDA can be applied to any analog pin‘’, while "The F2802x and F2803x devices do not have specific power sequencing requirements. " But in TMS320F2803x Real-Time Microcontrollers datasheet (Rev. P), it says ''No voltage larger than a diode drop (0.7 V) above VDDIO should be applied to any digital pin (for analog pins, this value is 0.7 V above VDDA) before powering up the device. '' Is there a conflict?