Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D
I have a signal on ADCINB5 that I want to use with the CMPSS. Since ADCINB5 does not share a pin with a CMPSS input, I connected ADCINB5 to ADCINA2, using the header pins on the LaunchPad. (J7-5 to J3-9)
What I have observed:
Under the no-load condition and with ADCINB5 disconnected from ADCINA2, I see an ADC measurement of 0x8CC.
When I connect ADCINB5 to ADCINA2, the ADCINB5 measurement jumps to ~0x8DB. The measurement at ADCINA2 is at ~0x88B.
- I did not expect the ADCINB5 measurement to change
- I expected that ADCINB5 would have the same measurement as ADCINA2
Launchpad revision is 2.0. (The note for Rev 1.1 about ADCINA2 being tied to VREFHI on Rev 1.1 should not apply)
ADCINA2 is not connected in this application. (The Launchpad is connected to a custom daughterboard, but ADCINA2 is not used)
I use SOC1 on ADCA for ADCINA2 and SOC1 on ADCB for ADCINB5.
SOC1 in both cases is triggered by EPWM6A
Any suggestions on why B5 does not match A2? Or why B5 changes when A2 is connected?
Thanks!