Part Number: F28M35H52C
Other Parts Discussed in Thread: UNIFLASH
Hi,
I have a question。
After I modified the send function of can.c under f28m35 driverlib, I can't upgrade the compiled bin file。
Please help me solve the problem。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: F28M35H52C
Other Parts Discussed in Thread: UNIFLASH
Hi,
I have a question。
After I modified the send function of can.c under f28m35 driverlib, I can't upgrade the compiled bin file。
Please help me solve the problem。
I will need some additional information to help you with this issue. Does CCS give some error when recompiling the project after you make the change? If so can you post the CCS error message?
Or do you have an issue programming the device with the new .out file?
Best,
Matthew
YaoWei,
Thank you for the additional information, some follow up questions.
Q1)Which JTAG debug probe are you using to connect to the device?
Q2)Is the C2000 on a custom PCB or a TI PCB?
Q3)Do many devices have this same issue or only one device? Have you tested multiple devices?
Q4)Do you have a F28M35 control CARD, and does Uniflash work correctly with it?
Best,
Matthew