Hello,
Just wondering if someone would be able to help me out with code composer version 4. I am currently building a project and i am in the debug stage but was wondering whether it is possible to view variables that constantly update.
Presently when i want to a view a variable i have to pause the running of the project for it to update but in the near future, this will not be able to happen due to the design of the project.
As a result of this i was wondering if there is a way to view variables that constantly update their value without having to pause the running of the project.
Cheers,