This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADCs' clocks divide by two

Hello TI,

I'm using the High Voltage Motor Control and PFC Developer's Kit (TMS320C28035) and my application requires ADC in more slowly mode. So i would like to divide by two (60/2 MHz) the system clock to ADC. I did that by code

EALLOW;

AdcRegs.ADCCTL2.all = 1;

EDIS; 

Hovewer, the real value in this register is still 0. I'm using the HVACI_Sensored example and above mentioned code I write in ADC_MACRO_INIT(). Please, can you write me if the values in that register can be changed?

Thank you,

Tom.