Hi team,
As per the GPIO chapter, GPIO42 and GPIO43 are Analog GPIOs i.e. can be configured as digital GPIO or Analog input. I can see GPBAMSEL register in GpioCtrlRegs. However, I cannot see the counterpart 'AGPIOCTRLB' in analog subsystem registers.
So if I want to use these GPIOs as an Analog input, which Analog subystem register should I refer?
Thanks and regards,
Irene