Part Number: TMS320F28388D
Hi Team,
1. When configuring classic CAN, we can use different mailbox configurations. For example, mailbox 1 is configured with a set of configurations, and mailbox 2 is configured with a set of configurations. There is no need to specifically configure a piece of RAM.
In CANFD, why is it necessary to configure a ram area to store these configurations? For example:
// // Initialize Message RAM Sections Configuration Parameters // msgRAMConfigParams.flssa = MCAN_STD_ID_FILT_START_ADDR; // Standard ID Filter List Start Address. msgRAMConfigParams.lss = MCAN_STD_ID_FILTER_NUM; // List Size: Standard ID. msgRAMConfigParams.rxBufStartAddr = MCAN_RX_BUFF_START_ADDR; // Rx Buffer Start Address. msgRAMConfigParams.rxBufElemSize = MCAN_RX_BUFF_ELEM_SIZE;
2. How to calculate the sending delay compensation parameters?
--
Thanks & Regards