Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE
Hi,
I want to use F28P650D in designing a three phase UPS. CPU1 doing the PFC and CPU2 doing the inverter. I would like to know if I can develop the entire PFC first for CPU1 as if it were a single core project and write the firmware to flash.
Then develop the firmware for the inverter, CPU2, as if it were another single core project. So that whenever I load the inverter firmware into the flash, I don't need to load the PFC firmware as well.
Would this procedure be possible?
Is there any C2000 application that uses dual core?
best regards,
Ari