Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
HI,
Selecting INTSOC2 as CLK source for SYSCLK and X1_XTAL for AUXCLK will fail CPU1 start because of the wrong used defines.
SysConfig selection:


And the generated code:


Line 120 should use DEVICE_AUXOSCSRC_FREQ = 25MHz but instead it uses DEVICE_OSCSRC_FREQ = 10MHz.
CCS Version: 12.5.0
C2000Ware version: 5.00.00.00
Compiler Version: 22.6.1.LTS