This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157: Arbitrary Reset

Part Number: TMS320F2800157

It appears that every part goes through a reset at some arbitrary time after power on.  We have seen it as soon as 100 seconds after power on and as late as 3 hours after power on.  Once the reset occurs, it doesn’t reset again.  In one test, the 5 samples reset at 166s, 1905s, 2722s, 6772s, and 10440s respectively.  The test was restarted at 415820s (115 hrs) but then after the restart, they all reset once again, but in different orders and at different times.  No part has ever reset 2x during the same power cycle.