This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28388D: TMDSCNCD28388D Evaluation kit not getting detected

Part Number: TMDSCNCD28388D

Hi Everyone,

We bought two evaluation boards TMDSCNCD28388D and we are facing a problem with the USB connectivity for one of the evaluation board. It is not getting detected. After comparing it with the other board with the same setup, we observed that the D5 led which is related to +3.3V on the board is not glowing. Below are attached snapshots of both the boards, first image shows working board and second image shows non-working board. Kindly provide support in resolving this issue.