This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear 2000 expert,
For F28002x and F28004x devices, there is a dcsm related asm and cmd files in C:\ti\c2000\C2000Ware_5_00_00_00\device_support\f28002x\common, but I didn't find any related source files for F28003x device.
I have done the DSCM for F28002x devices, so it will be very easy to realize this feature based on those related files.
Can you please help me know how to get those files for F28003x devices?
f28002x_dcsm_z1otp.asm
f28002x_dcsm_z2otp.asm
28002x_dcsm_lnk.cmd
Regards,
Jack
Jack,
The .asm and .cmd files are now in the diagnostic folder inside the sdl_ex_dcsm_ffi example folder in the C2000Ware - C2000Ware\libraries\diagnostic\f28003x\examples\sdl_ex_dcsm_ffi. We have a DCSM Security tool example in the release package. When we build the example, it will generate the corresponding .asm and .cmd files in the workspace\dcsm_security_tool\CPU1_RAM\syscfg folder.
You can also configure and program the security settings using the On-Chip Flash tool. Once you connect the device using CCS, open On-Chip Flash tool -> security settings, you can view the Zone 1 and Zone 2 settings.