Hi
I'm a new user of EVM: TMDSACDCKIT(C2000 AC/DC Developer's Kit). I was following the FBPS guide to run demo program provided. I used "BUILD 1" option(open loop FBPS). But I found some very strange thing.
If I apply 12V at J9, the 12V, 3.3V, 5V, 3.3V isolated are all ok. DSC can output PWM. I can monitor/change phase shift for practice. But if I add 15V at J26, J27, there is no PWM output. 12V, 3.3V, 5V, 3.3V isolated are all ok, too. On scope i can find the DSC stops output pwm signal just after 1-2 pwm signals. However, it sinks the same current as in normal operation condition(i.e 12V_aux-power added condition). I tried to test all points. And I found if I add 12V at U14 output, both TP73 or TP75 can make DSC output PWM normally. But if I move the input voltage at the beginning end, i.e, J26, J27. It doesn't work.
I think this is quite strange. Could anyone help me on this? Thanks in advance.
By the way, I asked where to add the aux-power before. Brett helped me. He suggested me use 5V. However, it seems this board has some options. For my board, the U17 is DCR011203U, so I have to use 12V as aux-power. Can anyone let me know why we have some small deviations on one EVM?
Thanks,
Violet