This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: a sampling issue while debugging with 280025

Part Number: TMS320F280025

Dear Expert

I encountered a sampling issue while debugging with 280025 .
The blue represents the actual output voltage of my entire machine at 12.2V, while the green represents the time it takes for my program to raise the IO port when it detects that the actual output voltage is less than 12.10V,
There are over 100 us in the middle delay, and the hardware circuit sampling uses resistor voltage divider. May I ask what may be the reason for my software ADC configuration sampling?
Currently, the timer 100K is used for triggering, and the ADC configuration code is as follows. Please help analyze it. Thank you, there is no delay from the hardware signal to the DSP analog port.

static void sInitAdc(void)

{   

//ADCA clock

EALLOW;

CpuSysRegs.PCLKCR13.bit.ADC_A

= 1;

   // CpuSysRegs.PCLKCR13.bit.ADC_B = 1;

    CpuSysRegs.PCLKCR13.bit.ADC_C = 1;

// Device_cal(); //bootrom会调用,这里是避免仿真时不执行bootrom

EDIS;

 

//ADC 参考电压3.3V

SetVREF(ADC_ADCA, ADC_INTERNAL, ADC_VREF3P3);

//SetVREF(ADC_ADCB, ADC_INTERNAL, ADC_VREF3P3);

SetVREF(ADC_ADCC, ADC_INTERNAL, ADC_VREF3P3);

DELAY_US(1000);

 

    EALLOW;

    AdcaRegs.ADCCTL2.bit.PRESCALE = 6;

    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;//转换结束产生事件

 

    //3200W LLC

AdcaRegs.ADCSOC0CTL.bit.CHSEL = 3;//temp AMB

AdcaRegs.ADCSOC1CTL.bit.CHSEL

= 1;

AdcaRegs.ADCSOC2CTL.bit.CHSEL

= 12;//temp SEC

AdcaRegs.ADCSOC3CTL.bit.CHSEL

= 2;

AdcaRegs.ADCSOC4CTL.bit.CHSEL

= 5;

AdcaRegs.ADCSOC5CTL.bit.CHSEL

= 4;//输出电流采样

AdcaRegs.ADCSOC6CTL.bit.CHSEL

= 15;

AdcaRegs.ADCSOC7CTL.bit.CHSEL

= 6;

AdcaRegs.ADCSOC8CTL.bit.CHSEL

= 3;//输出电压采样

 

    AdcaRegs.ADCSOC0CTL.bit.ACQPS = 9;//Sample window is 10 SYSCLK cycles

AdcaRegs.ADCSOC1CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC2CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC3CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC4CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC5CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC6CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC7CTL.bit.ACQPS = 9;

AdcaRegs.ADCSOC8CTL.bit.ACQPS = 9;

 

//tbd

    AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 2;//CpuTimer1  fs=100k

    AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC3CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC4CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC5CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC6CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC7CTL.bit.TRIGSEL = 2;

AdcaRegs.ADCSOC8CTL.bit.TRIGSEL = 2;

 

//tbd

    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 8;// End of SOC0 will set INT1 flag

    AdcaRegs.ADCINTSEL1N2.bit.INT1E = 0;// Enable INT1 flag

    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;// Make sure INT1 flag is cleared

AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;//power up

    EDIS;

 

//ADCB

    EALLOW;

    AdccRegs.ADCCTL2.bit.PRESCALE = 6;

    AdccRegs.ADCCTL1.bit.INTPULSEPOS = 1;//转换结束产生事件

 

AdccRegs.ADCSOC0CTL.bit.CHSEL = 1;//ADDR2

AdccRegs.ADCSOC1CTL.bit.CHSEL = 4;//VFB

AdccRegs.ADCSOC2CTL.bit.CHSEL = 10;//IFB

    AdccRegs.ADCSOC0CTL.bit.ACQPS = 9;//Sample window is 10 SYSCLK cycles

AdccRegs.ADCSOC1CTL.bit.ACQPS = 9;

AdccRegs.ADCSOC2CTL.bit.ACQPS = 9;

 

//tbd

    AdccRegs.ADCSOC0CTL.bit.TRIGSEL = 2;//CpuTimer1  fs=83k

    AdccRegs.ADCSOC1CTL.bit.TRIGSEL = 2;

AdccRegs.ADCSOC2CTL.bit.TRIGSEL = 2;

 

AdccRegs.ADCINTSEL1N2.bit.INT1SEL = 2;// End of SOC2 will set INT1 flag

    AdccRegs.ADCINTSEL1N2.bit.INT1E = 0;// Enable INT1 flag

    AdccRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;// Make sure INT1 flag is cleared

AdccRegs.ADCCTL1.bit.ADCPWDNZ = 1;//power up

    EDIS;

    DELAY_US(1000);

 

//PIE

//EALLOW; //diable

//PieVectTable.ADCA1_INT

= &ADCA1_ISR;  //tbd

//EDIS;

//PieCtrlRegs.PIEIER1.bit.INTx1 = 1;

//IER |= M_INT1;

}

  • Hi Gabriel,

    Sorry,  I don't fully understand the CPU timer setting that triggers the ADC conversion.  You mentioned 100K for timer. Is the timer set to generate the SOC every 100K SYSCLK cycles?  At 100MHz SYSCLK, ADC will trigger every 1ms (10ns * 100K).

    Some observations on the ADC settings:

              - Prescale setting is set to 6.  This means that ADC is running with SYSCLK/4 or 25MHz (100MHz/4), which is only half the rated ADC speed of 50MHz

              - ADC sampling (ACQPS) is set to 9 which is 10 (9+1) SYSCLK times or 100ns.  If the 12.2v is scaled down to 3.3V level for the ADC by a voltage divider, there series resistor and any filter capacitance would produce a very high impedance seen at the ADC channel.  This may be greater than 50ohms/100pF.  An ACQPS of 9 will not be enough to settle the ADC input voltage for proper sampling (see  "Choosing an Acquisition Window Duration" chapter in the TRM regarding sampling/settling when input impedances are taken into account)

    Regards,

    Joseph