This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Demo for 28335



Hi,

I am working for a company.We are planning to use 28335 kit for one of my applications.

Can any TI person give demo in our company?

When we try to ask them for demo, they keep on telling that they are busy.

Can ant one suggest in this regard?

  • Nisanth,

     

    Are you running into technical difficulties with the 28335 Experimenter kit? 

     

    Regards,

    Michael Wei

    C2000 Product Marketing

  • Sir,

    I didnt get wat u r askin.

    I am working in Bangalore, India. I want to use 28335 in analysis of DC ripple current (from  three phase full  bridge converter ).  The DC ripple has peak value of around 100 V. I am using hall sensor to bring the voltage level down to 3.2 volts compatible with MCUs.

    But i am not comfortable with MCUs. So i want to have a demo from TI-Bangalore (India) people.  I am expecting a demo consists of basics showing accepting external signals (sinusoidal for ex.,) to ADC, its interface with MCUs, how we can retrieve that data samples back in programming, driving a relay ( through relay driver circuit) etc.,

    But i am not getting any help in this regard. Although there is scope for huge order of these kits from our side in future after we succeed, i couldn't understand the cause of the delay. We have been requesting for the past one month.

    Kindly help in this regard.