Part Number: TMS320F28379D
Hi there
Could you please review the SPI Flash connection with TMS320F28379D product ?
Flash PN: W25Q128JVPIM
CS Flash pin: GPIO49
MOSI Flash pin: GPIO50
MISO Flash pin: GPIO51
SCLK Flash pin: GPIO52

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379D
Hi there
Could you please review the SPI Flash connection with TMS320F28379D product ?
Flash PN: W25Q128JVPIM
CS Flash pin: GPIO49
MOSI Flash pin: GPIO50
MISO Flash pin: GPIO51
SCLK Flash pin: GPIO52

Hi,
Our SME is currently OOO and will revert once he resumes office. Please expect delays in response, regret for inconvenience.
Regards,
Rajeshwary
Hi,
CS Flash pin: GPIO49
You could use GPIO53 for SPISTEC signal (CS) controlled by SPI C module. Otherwise you will have to control the CS pin yourself using GPIO writes.
For WP signal you plan to have just a pull-up or down (i..e de-pop R60 or R62)? Currently the schematic shows a voltage divider on the pin.
Best,
Kevin