Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG
Hi Champ,
I am asking for my customer.
As the PMBus module has to two modes, PMBus mode and I2C mode. It is known that PMBus mode could have multiple slave address support.
(1). Does the PMBus over I2C also hw support multiple slave address ? From sysconfig GUI, after checking the enable I2C mode checkbox, if the device is configured as target mode in PMBus device mode, it is grayed out for the masked addresses displayed in binary. May I reconfirm that ?
(2). Continue to 1st question, if not, any sw workaround to achieve multiple slave address in I2C mode ?
(3). The PMBus example we have now (located at libraries\communications\PMBus), it is included a library (F28003x_PMBus_Communications_Stack_Over_I2C.lib) and be called in the example (pmbus_stack_over_i2c_project) , do we have a plan to disclose it, and for customer could direct control of underlying registers of PMBus ?
Thanks and regards,
Johnny