Part Number: TMS320F28374D
i need to interface. DMA over USB2.0(micro usb) for transfer data and i need to transfer 100 bytes of data at a time in 15 micro/sec.
please help me for achieving for this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28374D
i need to interface. DMA over USB2.0(micro usb) for transfer data and i need to transfer 100 bytes of data at a time in 15 micro/sec.
please help me for achieving for this.
Hi,
The DMA is not correctly intergrated with USB and hence the USB trigger signals are not supported on this device. There is an errata due to which USB module generates inadvertent extra DMA requests, causing the FIFO to overflow or underflow.
Best Regards
Siddharth