This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: MCU063B Documentation Discrepancy

Part Number: TMS320F28388D


Greetings,

I have set up our MCU063B to start debugging code.  According to the directions in spruil8b section 2, option 1 says that D3 should illuminate.  But according to the schematic, D3 is a Schottky diode, not an LED.  An examination of the board confirms that it is not an LED.  However, D5, which illuminates when the 3V3 supply is running, does illuminate using both options.  So I’m assuming that D3 in the document is a typo, and should be D5?

Thank you,

Ed