Part Number: TMS320F280049-Q1
Other Parts Discussed in Thread: UNIFLASH
Dear Champs,
I am asking this for our customer.
The user has used Uniflash with one XDS110 for mass production.
Now, the user is thinking to use Uniflash to connect to two or even more XDS110 for programming.
For example, if they just use two XDS110 for programming,
Does Uniflash support multiple XDS110 programming by the serial number below?
If yes, can they also do this in command line?
How do they modify the command line package to implement these?