Part Number: TMS320F28379D
Hello Experts,
I am configuring ADC A, B, and C in single-ended mode triggering with TIMER2 every 100uS. I see that the ADCs are triggering only once. I tried keeping break point in ISR and see that its hitting only once. Just to confirm, I added some led blink code in the timer ISR which is working fine. But ADCs are not triggering.
I am attaching the code. Can you please tell me what's wrong here?
// Main.c
//#############################################################################
//
// FILE: led_ex1_blinky.c
//
// TITLE: LED Blinky Example
//
//! \addtogroup driver_example_list
//! <h1> LED Blinky Example </h1>
//!
//! This example demonstrates how to blink a LED.
//!
//! \b External \b Connections \n
//! - None.
//!
//! \b Watch \b Variables \n
//! - None.
//!
//
//#############################################################################
// $TI Release: F2837xD Support Library v3.11.00.00 $
// $Release Date: Sun Oct 4 15:55:24 IST 2020 $
// $Copyright:
// Copyright (C) 2013-2020 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "header.h"
uint16_t _timer_1SEC = 0;
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
//
Device_init();
Device_initGPIO();
GPIO_setPadConfig(166, GPIO_PIN_TYPE_STD);
GPIO_setDirectionMode(166, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(167, GPIO_PIN_TYPE_STD);
GPIO_setDirectionMode(167, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(168, GPIO_PIN_TYPE_STD);
GPIO_setDirectionMode(168, GPIO_DIR_MODE_OUT);
Init_ADCs(); //Initialize ADC's & Initialize SOC's
Init_ADC_SOCs();
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
Interrupt_register(INT_ADCA1, &ADCA_ISR);
Interrupt_enable(INT_ADCA1);
Interrupt_register(INT_ADCB1, &ADCB_ISR);
Interrupt_enable(INT_ADCB1);
Interrupt_register(INT_ADCC1, &ADCC_ISR);
Interrupt_enable(INT_ADCC1);
Interrupt_register(INT_TIMER2, &TIMER2_ISR);
INIT_CPU_TIMERS();
Config_CPU_TIMER(CPUTIMER2_BASE, DEVICE_SYSCLK_FREQ, 100);
CPUTimer_enableInterrupt(CPUTIMER2_BASE);
Interrupt_enable(INT_TIMER2);
CPUTimer_startTimer(CPUTIMER2_BASE);
//
// Loop Forever
//
for (;;)
{
IRX_PP = (IRX_PP_BUFFER * 18.182 / 4096.0) - 9.091;
I_RX_INST = (ADC_I_RX_INST * 18.182 / 4096.0) - 9.091;
}
}
//
// End of File
//
//Analog.h
/*
* Analog.h
*
* Created on: 16-Sep-2021
* Author: Vishal
*/
// +-+-+-+-+-+-+-+ +-+-+-+-+-+-+ +-+-+-+-+-+-+
// |A|u|t|h|o|r|:| |V|i|s|h|a|l| |K|a|k|a|d|e|
// +-+-+-+-+-+-+-+ +-+-+-+-+-+-+ +-+-+-+-+-+-+
// ____ ____ ____ ____ ____ ____ ___ __
///\ _`\ /\ _`\ /\ _`\ /\ _`\ /\ _`\ /\ _`\ /'___`\ /'__`\
//\ \ \L\_\ \ \L\ \ \ \L\ \ \ \ \L\ \ \ \L\ \ \,\L\_\ /\_\ /\ \ /\ \/\ \
// \ \ _\L\ \ ,__/\ \ , / \ \ ,__/\ \ ,__/\/_\__ \ \/_/// /__ \ \ \ \ \
// \ \ \L\ \ \ \/ \ \ \\ \ \ \ \/ \ \ \/ /\ \L\ \ // /_\ \__\ \ \_\ \
// \ \____/\ \_\ \ \_\ \_\ \ \_\ \ \_\ \ `\____\ /\______/\_\\ \____/
// \/___/ \/_/ \/_/\/ / \/_/ \/_/ \/_____/ \/_____/\/_/ \/___/
//
#ifndef ANALOG_H_
#define ANALOG_H_
//********************************** Analog Signals*************************************
extern uint16_t ADC_IRX_PP;
extern uint16_t ADC_I_RX_INST;
extern float IRX_PP;
extern float I_RX_INST;
extern uint16_t ADCIN14_3V;
extern uint16_t ADCIN15_0V;
extern uint16_t IRX_PP_BUFFER;
extern uint16_t ADCINB0;
extern uint16_t ADCINB1;
void Init_ADCs(void);
void Init_ADC_SOCs(void);
//********** Functions to Read ADC's**************
__interrupt void ADCA_ISR(void);
__interrupt void ADCB_ISR(void);
__interrupt void ADCC_ISR(void);
__interrupt void TIMER2_ISR(void);
void INIT_CPU_TIMERS(void);
void Config_CPU_TIMER(uint32_t, float, float);
#endif /* ANALOG_H_ */
//Analog.c
/*
* Config_ADC.c
*
* Created on: 02-Dec-2019
* Author: Vishal
*/
// +-+-+-+-+-+-+-+ +-+-+-+-+-+-+ +-+-+-+-+-+-+
// |A|u|t|h|o|r|:| |V|i|s|h|a|l| |K|a|k|a|d|e|
// +-+-+-+-+-+-+-+ +-+-+-+-+-+-+ +-+-+-+-+-+-+
// ____ ____ ____ ____ ____ ____ ___ __
///\ _`\ /\ _`\ /\ _`\ /\ _`\ /\ _`\ /\ _`\ /'___`\ /'__`\
//\ \ \L\_\ \ \L\ \ \ \L\ \ \ \ \L\ \ \ \L\ \ \,\L\_\ /\_\ /\ \ /\ \/\ \
// \ \ _\L\ \ ,__/\ \ , / \ \ ,__/\ \ ,__/\/_\__ \ \/_/// /__ \ \ \ \ \
// \ \ \L\ \ \ \/ \ \ \\ \ \ \ \/ \ \ \/ /\ \L\ \ // /_\ \__\ \ \_\ \
// \ \____/\ \_\ \ \_\ \_\ \ \_\ \ \_\ \ `\____\ /\______/\_\\ \____/
// \/___/ \/_/ \/_/\/ / \/_/ \/_/ \/_____/ \/_____/\/_/ \/___/
//
// This file contains Functions to initialize ADC's , Initialize start of Conversions, & Read All the RAW values of Analog Signals.
#include"header.h"
//Initialize the analog results.
//********** Analog Signals*************
uint16_t ADC_IRX_PP = 0;
uint16_t ADC_I_RX_INST = 0;
float IRX_PP = 0.0;
float I_RX_INST = 0.0;
extern uint16_t ADCIN14_3V = 0;
extern uint16_t ADCIN15_0V = 0;
uint16_t IRX_PP_BUFFER = 0;
uint16_t ADCINB0 = 0;
uint16_t ADCINB1 = 0;
//********** Initialize ADC's*************
void Init_ADCs(void)
{
//
// Set ADCCLK divider to /4
//
ADC_setPrescaler(ADCA_BASE, ADC_CLK_DIV_4_0);
ADC_setPrescaler(ADCB_BASE, ADC_CLK_DIV_4_0);
ADC_setPrescaler(ADCC_BASE, ADC_CLK_DIV_4_0);
//
// Set resolution and signal mode (see #defines above) and load
// corresponding trims.
//
ADC_setMode(ADCA_BASE, ADC_RESOLUTION_12BIT, ADC_MODE_SINGLE_ENDED);
ADC_setMode(ADCB_BASE, ADC_RESOLUTION_12BIT, ADC_MODE_SINGLE_ENDED);
ADC_setMode(ADCC_BASE, ADC_RESOLUTION_12BIT, ADC_MODE_SINGLE_ENDED);
//
// Set pulse positions to late
//
ADC_setInterruptPulseMode(ADCA_BASE, ADC_PULSE_END_OF_CONV);
ADC_setInterruptPulseMode(ADCB_BASE, ADC_PULSE_END_OF_CONV);
ADC_setInterruptPulseMode(ADCC_BASE, ADC_PULSE_END_OF_CONV);
//
// Power up the ADCs and then delay for 1 ms
//
ADC_enableConverter(ADCA_BASE);
ADC_enableConverter(ADCB_BASE);
ADC_enableConverter(ADCC_BASE);
DEVICE_DELAY_US(1000);
}
//
// Function to configure Start of conversion (SOC) for ADC's
//
void Init_ADC_SOCs(void)
{
// - For 12-bit resolution, a sampling window of 15 (75 ns at a 200MHz
// SYSCLK rate) will be used. For 16-bit resolution, a sampling window
// of 64 (320 ns at a 200MHz SYSCLK rate) will be used.
//
ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER2, ADC_TRIGGER_CPU1_TINT2,
ADC_CH_ADCIN2, 15);
ADC_setInterruptSource(ADCA_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER2);
ADC_enableInterrupt(ADCA_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
/*
* ****************************************************************************
*/
ADC_setupSOC(ADCB_BASE, ADC_SOC_NUMBER0, ADC_TRIGGER_CPU1_TINT2,
ADC_CH_ADCIN0, 15);
ADC_setupSOC(ADCB_BASE, ADC_SOC_NUMBER1, ADC_TRIGGER_CPU1_TINT2,
ADC_CH_ADCIN1, 15);
ADC_setInterruptSource(ADCB_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER1);
ADC_enableInterrupt(ADCB_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCB_BASE, ADC_INT_NUMBER1);
/*
* ****************************************************************************
*/
ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER2, ADC_TRIGGER_CPU1_TINT2,
ADC_CH_ADCIN2, 15);
ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER14, ADC_TRIGGER_CPU1_TINT2,
ADC_CH_ADCIN14, 15);
ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER15, ADC_TRIGGER_CPU1_TINT2,
ADC_CH_ADCIN15, 15);
ADC_setInterruptSource(ADCC_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER15);
ADC_enableInterrupt(ADCC_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);
}
//
// ADC A Interrupt 1 ISR
//
__interrupt void ADCA_ISR(void)
{
ADC_IRX_PP = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER2);
if (ADC_IRX_PP > IRX_PP_BUFFER)
{
IRX_PP_BUFFER = ADC_IRX_PP;
// IRX_PP = (IRX_PP_BUFFER * 18.182 / 4096.0) - 9.091;
}
if (true == ADC_getInterruptOverflowStatus(ADCA_BASE, ADC_INT_NUMBER1))
{
ADC_clearInterruptOverflowStatus(ADCA_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
}
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}
__interrupt void ADCB_ISR(void)
{
// Store results
ADCINB0 = ADC_readResult(ADCBRESULT_BASE, ADC_SOC_NUMBER0);
ADCINB1 = ADC_readResult(ADCBRESULT_BASE, ADC_SOC_NUMBER1);
if (true == ADC_getInterruptOverflowStatus(ADCB_BASE, ADC_INT_NUMBER1))
{
ADC_clearInterruptOverflowStatus(ADCB_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCB_BASE, ADC_INT_NUMBER1);
}
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}
__interrupt void ADCC_ISR(void)
{
// Store results
ADC_I_RX_INST = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER2);
ADCIN14_3V = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER14);
ADCIN15_0V = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER15);
if (true == ADC_getInterruptOverflowStatus(ADCC_BASE, ADC_INT_NUMBER1))
{
ADC_clearInterruptOverflowStatus(ADCC_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);
}
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}
//Timer 2 comfigured to interrupt every 100uS
__interrupt void TIMER2_ISR(void)
{
_timer_1SEC++;
if (_timer_1SEC >= 10000)
{
_timer_1SEC = 0;
GPIO_togglePin(166);
GPIO_togglePin(167);
GPIO_togglePin(168);
}
}
void Config_CPU_TIMER(uint32_t cpuTimer, float freq, float period)
{
uint32_t temp;
temp = (uint32_t) (freq / 1000000 * period);
CPUTimer_setPeriod(cpuTimer, temp);
CPUTimer_setPreScaler(cpuTimer, 0);
CPUTimer_stopTimer(cpuTimer);
CPUTimer_reloadTimerCounter(cpuTimer);
CPUTimer_setEmulationMode(cpuTimer,
CPUTIMER_EMULATIONMODE_STOPAFTERNEXTDECREMENT);
CPUTimer_enableInterrupt(cpuTimer);
}
void INIT_CPU_TIMERS(void)
{
CPUTimer_setPeriod(CPUTIMER2_BASE, 0xFFFFFFFF);
CPUTimer_setPreScaler(CPUTIMER2_BASE, 0);
CPUTimer_stopTimer(CPUTIMER2_BASE);
CPUTimer_reloadTimerCounter(CPUTIMER2_BASE);
}
//header.h
/*
* header.h
*
* Created on: 28-Oct-2021
* Author: Vishal
*/
// +-+-+-+-+-+-+-+ +-+-+-+-+-+-+ +-+-+-+-+-+-+
// |A|u|t|h|o|r|:| |V|i|s|h|a|l| |K|a|k|a|d|e|
// +-+-+-+-+-+-+-+ +-+-+-+-+-+-+ +-+-+-+-+-+-+
// ____ ____ ____ ____ ____ ____ ___ __
///\ _`\ /\ _`\ /\ _`\ /\ _`\ /\ _`\ /\ _`\ /'___`\ /'__`\
//\ \ \L\_\ \ \L\ \ \ \L\ \ \ \ \L\ \ \ \L\ \ \,\L\_\ /\_\ /\ \ /\ \/\ \
// \ \ _\L\ \ ,__/\ \ , / \ \ ,__/\ \ ,__/\/_\__ \ \/_/// /__ \ \ \ \ \
// \ \ \L\ \ \ \/ \ \ \\ \ \ \ \/ \ \ \/ /\ \L\ \ // /_\ \__\ \ \_\ \
// \ \____/\ \_\ \ \_\ \_\ \ \_\ \ \_\ \ `\____\ /\______/\_\\ \____/
// \/___/ \/_/ \/_/\/ / \/_/ \/_/ \/_____/ \/_____/\/_/ \/___/
//
#ifndef HEADER_H_
#define HEADER_H_
#include "driverlib.h"
#include "device.h"
#include"Analog.h"
extern uint16_t _timer_1SEC;
//* Definition of standard bits *
//******************************************************************************/
#define BIT0 (uint16_t)(0x0001)
#define BIT1 (uint16_t)(0x0002)
#define BIT2 (uint16_t)(0x0004)
#define BIT3 (uint16_t)(0x0008)
#define BIT4 (uint16_t)(0x0010)
#define BIT5 (uint16_t)(0x0020)
#define BIT6 (uint16_t)(0x0040)
#define BIT7 (uint16_t)(0x0080)
#define BIT8 (uint16_t)(0x0100)
#define BIT9 (uint16_t)(0x0200)
#define BITA (uint16_t)(0x0400)
#define BITB (uint16_t)(0x0800)
#define BITC (uint16_t)(0x1000)
#define BITD (uint16_t)(0x2000)
#define BITE (uint16_t)(0x4000)
#define BITF (uint16_t)(0x8000)
#define BIT(x) ((uint16_t)1 << (x))
//******************************END OF NEW CODE****************************************
#endif /* HEADER_H_ */
Regards
Vishal Kakade