Part Number: TMS320F28335
The following warning appears in ccs10.1.0. How can I solve it?
1.“Description Resource Path Location Type
#10247-D creating output section ".cio" without a SECTIONS specification DSP2833x_mpu9250chuanjieya C/C++ Problem”
2.“Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 6.2.0 [C2000]. Another version of the compiler will be used during build - 20.2.1.LTS. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="">software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. DSP2833x_mpu9250chuanjieya properties Problem”