Part Number: TMS320F28027
Other Parts Discussed in Thread: MOTORWARE
Hi Team,
Here are two issues from the customer may need your help:
C:\ti\motorware\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\boostxldrv8305_revA\f28x\f2802xF\projects\ccs\proj_lab11a
1. 
#define USER_IQ_FULL_SCALE_CURRENT_A (24.0) // BOOSTXL-DRV8305EVM = 24.0 A
High lighted content in above screen shot mentioned the necessary conditions:
USER_IQ_FULL_SCALE_VOLTAGE_V > 0.5 * USER_MOTOR_MAX_CURRENT * USER_MOTOR_Ls_d * USER_VOLTAGE_FILTER_POLE_rps
If 24.0 is too small, what should it be set to? After changing it, the voltage sampling multiple is wrong.
2. 
The current of 24 is also too small. What should it be set to? Can it be doubled? Does the sampling part also need to be modified?

Is it changed here? What is the function of this IQ12mpy()?
--
Thanks & Regards