hello
I want to write data to tms320f240pqa internal flash
Current target <-> xds510usb <-> ccs3.3 connection succeeded
However, the ccs3.3 program cannot write data to flash.
I am trying to write to the internal flash using sdflash.
1. After running sdflash, I would like to insert the driver file into the target section of the settings menu. Can you send me what file corresponds to f240?
2. Can you send me the algorithm .out file for the erase, program, and verify items in the tab menu? This is the algorithm file corresponding to tms320f240pqa.
When I searched the forum, there was an algorithm file corresponding to f243, but I could not find an algorithm file corresponding to f240.
Does anyone have the file please?
thank you