Part Number: TMS320F28335
What is the difference between MPN: TMS320F28335PTPS and SM320F28335PTPS
Are they available ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
What is the difference between MPN: TMS320F28335PTPS and SM320F28335PTPS
Are they available ?
Thanks
Sagar,
TMS320F28335PTPS is the commercial version (–40°C to 125°C). SM320F28335PTPS operates at extended temperature ranges (-55°C to 150°C) and is much more expensive. Please refer to the respective device datasheets for more information. Yes, they are available.