Part Number: TMS320F28067
Hi team,
It works fine after using the simulator to program, and everything works fine after unplugging the simulator.
However, after re-powering on, the preset running lights and communication with the host computer are normal, but after using the host computer to start the wave and closed-loop control, the program is abnormal.
I thought it was a problem with the program boot at first, but both the communication and the running lights are normal.
Could you please help to analyze possible reasons? Thanks!
IC: TMS320F28067
Simulator: YXDSP-XDS100V3