Part Number: TMS320F280025
Hello,
I'm currently using motor control SDK for my own bard.
Software is based on universal motor control lab and I have several question on this:
-only _FULL_FAST_LIB seems to work, user_mtr1.c seems not compatible with other FAST_LIB.
Can you confirm if the other libs are functionnals? My need is for a PMSM and I try to reduce the size of the code. If yes can you please advice what is needed?
-ADC PPB are configured but I can not see where it is used. I cannot see any PPB event or interupt used in the code. Can you please let me know why PPB is used?
-On another post on the forum I read that UL approval was in progress, do you have some updates on this?
With best regards.