Other Parts Discussed in Thread: SYSBIOS, CONTROLSUITE
Hi Team,
There's an issue from the customer need your help:
Due to the needs of the requirements, I used Matlab automatic code generation in CPU1 and SYS/BIOS operating system in CPU2 (I used two components Clock and Hwi, and I observed whether the components were working properly by lighting the breathing lamp), and found the following problems after the writing was completed:
1) In debug mode, I run CPU1 and then CPU2, and the whole system can run normally, (observe that the breathing light can run normally), but in this case, if I power on again, CPU1 can run normally, and CPU2 can only complete initialization, and cannot enter the Hwi, Clock task.
2) In debug mode, if I run CPU2 first and then CPU1, the report is wrong, and the initialization of CPU2 cannot be completed.
I don't have a deep understanding of the SYS/BIOS initialization process, and I don't have too much information to explain, so I hope to be able to explain it in detail.
Component versions used:
CCS12.1
SYSbios:6.83.0.18
XDCtools:3.62.1.16
Library functions:
controlsuite:v190F2873xD
Best Regards,
Ben