Other Parts Discussed in Thread: MOTORWARE
Hi Ti team:
I am running the universal motor control programm with tms320f2800157 for LEVEL 4.
I found the start profile is different with previous instaspin foc .
Can you help to provide suggestions for how to tunning the start profile , for example how to quickly enter into speed closeloop ,decrease the currentloop time.
There are two pictures as below , the left is current start profile with universal motor control lab ,,the right is previous instaspin start profile .
how can I tunning the current software(universal motor control lab) to meet the right start profile .


Also please help to explain the meaning of the below parameters
// the speed threshold for start the motor, in Hz
#define USER_MOTOR1_SPEED_START_Hz (35.0f) // Hz
// the speed threshold for running the motor with force open-loop, in Hz
#define USER_MOTOR1_SPEED_FORCE_Hz (30.0f) // Hz