Part Number: TMS320F28377D
Hi
When I was using the ADC of thee DSP, the digital result exhibits a large peak, not regularly.
If I tried to enlarge the S/H value in the configuration of the ADC resigister, things turns worse. The best sampling performance is shown as the following figure. Is there any possible reason for this phenomenon?
The phase-to-phase voltage is sampled by an isolate transformer. I have talso ried to use the differential routing to sampling the phase-to-phase voltage, the amplifier is aslo replaced by higher CMR>80dB. The RC fitler at the output of the OA is 100ohm and 1nF, and the RC filter at the input of the ADC is 10ohm and 10nF.