Part Number: TMS320F280049C
We are working on a 2 phases DCDC converter using 2 TMS320F280049C DSPs.
We have connected the output current sensing of phase1 to A0 Analog input on DSP1 to A2 Analog input on DSP2.
While booth DSPs are Powered On booth are reading a correct value, but when we power Off DSP2, DSP1 is reading a wrong value, and we read near to 40% of the real value.
Looks like DSP2 is somehow adding an unexpected impedance that is affecting the voltage connected to A0 on DSP1.
Can you explain the behavior of A2 pin during a Power Off sequence?