This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280033: C2000-GANG programming

Part Number: TMS320F280033

I want to write to TMS320F280033 using C2000-GANG.

Select TMS320F280033.

 

When I load the data

Error 396: Warning: Code in file is outside the range of the selected MCU.

This is what you will see when you open memory options.

The flash start address is 0x080000 and the flash end address is 0x8FFFF.

According to the specification, the correct address ranges are:

The flash start address is 0x088000 and the flash end address is 0x97FFF.

I think there is something wrong with this setting, so please give me some advice on what to do.